2016-01-21 11:00 PM
Hi
I have the STEVAL-IHM032V1 and STEVAL-IHM039V1.The motor is T-motor U8. I have configure the U8 through ST Motor Control Workbeach. The Keil has build success.But the motor is not work. I use the Oscilloscope to see the six PWM from IHM039V1, The PWM has no response。 When I debug in the keil,it stop in the MCboot(oMCI,oMCT).The Serial communication is not connect the IHM039V1. Thanks .