cancel
Showing results for 
Search instead for 
Did you mean: 

steval-esc001v1 not detected

srinath mallikarjunan
Associate II
Posted on July 06, 2018 at 11:51

Hi

I try to connect to the board using STLink-v2 using IAR. But i get an error that device is not connected.

Board is powered from a 12V source. 

PWM lines are unconnected.

What could be the problem ?

#steval-esc001v1
2 REPLIES 2
kyrreaa
Associate III
Posted on July 10, 2018 at 15:20

I've also had this problem until I found my connector pinning was reversed.

Check your pinnings again and again. You never know until you check twice.

srinath mallikarjunan
Associate II
Posted on July 11, 2018 at 13:35

Yes that was it..

I wish the picture they provide in the PDF was clearer.