cancel
Showing results for 
Search instead for 
Did you mean: 

L6699D No load condition

Patrick Winter
Associate
Posted on July 11, 2018 at 14:49

Hi All,

I have a 500W PS build around the L6699D and everything is working good.

Now I found 1 little thing:

If I run the unit in No Load the output is 24Vdc if I take the input voltage (AC) away the output drops a little.

Now if I switch the unit back on the output voltage flies up and clamps to the OVP (30Vdc) and it is unable to regulate the voltage down despite that the signals are there.

Now my question is, is this someting I can control or is this a problem in the L6699D?

Hope someone can help me.

Thanks,

Patrick

#l6699d-no-load
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0