cancel
Showing results for 
Search instead for 
Did you mean: 

STEF05: What is the minimum time En/Fault must be held low to reset the device?

RBerw.1
Associate II
 
3 REPLIES 3
Peter BENSCH
ST Employee

Usually you would reset the STEF05 using e.g. a MOSFET, as shown in the datasheet, fig. 4.

The datasheet gives a recommendation how to handle the Enable/Fault pin (section 5.4): "[...]the device can be reset either by cycling the supply voltage or by pulling down the Enable pin below the Vil threshold and then releasing it."

The datasheet also contains the value of Vil.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
RBerw.1
Associate II

Just to confirm; There is no minimum timing, reset occurs immediately when Enable/Fault is pulled below Vil?

Peter BENSCH
ST Employee

Correct.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.