2011-12-09 8:03 AM
Hello
Themotor kit
comes with
the motor
MCKIT
LA052
-
080E3NL1Shinano
.Phase
0.60
ohm
resistance
Inductance
1.4
mH
Phase
Back
EMF
constant
Kv
6.2
/
krpm
However, in the
motor
parameter
''
workbench
motor control
''sets.
Motor
winding
resistance
RS
(phase
) 0.35ohm
Synchronous
Motor
winding
inductance
Ls
(
phase)0.6mH
B-
EmfConstant
(Vrms
/
krpm
) 4kv /
krpm
I would need
an explanation of the
conversion
performed.
Best regards
2011-12-20 12:14 AM
Hello Jokin,
No conversions have been in fact performed... I'd recommendt to measure parameters rather than refer to the datasheet ones (sometime you can see some discrepancies). Parameters really set in ST MC Workbench have been actually measured directly on the motor terminals. Best Regards, Billino