Skip to main content
sebastianr
Associate II
December 7, 2011
Question

ST MC workbench parameters

  • December 7, 2011
  • 2 replies
  • 475 views
Posted on December 07, 2011 at 15:03

Hi,

Im completely new to the topic of motor control with STM32 devices. To get started, I chose the STM3210E-EVAL board, the STEVAL-IHM031V1 driver board and an appropriate BLDC.

Now Im trying to generate the parameter headers and sources with the motor control workbench matching my hardware. The problem is, that I can't find all neccessary parameters for the power stage, e.g. temperature sensing, params of the MOSFET power switches (dead-time, switching frequency) ... to name but a few. Neither the user manuals of the boards nor the data sheets of the particular components contain these parameters. Where can I get them?

thanks in advance!

regards,

sebastian
This topic has been closed for replies.

2 replies

bille.stello
Associate
December 19, 2011
Posted on December 19, 2011 at 17:29

Hello Sebastian,

I agree with you, ST should provide for the STEVAL boards the parameters required by ST MC Workbench PC SW. I'm sure thy're already working on it ;)

By the way, for the time being, I'm attaching my personal notes taken in the lab and listing the parameters you required for some of the ST boards. I hope there are no errors!

Best Regards,

Billino

sebastianr
Associate II
December 21, 2011
Posted on December 21, 2011 at 12:47

Thanks alot, very helpful!

regards,

sebastian