cancel
Showing results for 
Search instead for 
Did you mean: 

SOF-IRQ when cascading 3 devices of LED1202

Gera.V
Associate

Hi,

what is the behaviour of the IRQ-Lines of the LED1202 when connected wired-OR as in chapter 6.2 of datasheet (i.e. clock synchronized 1x Master, 2x Slaves)? I want to use SHFT=1 on all 3 devices.

As per datasheet, the update of the PWM - registers has to be synchronized to the SOF-interrupt to avoid PWM artifacts.

But beeing all 3x IRQ's wired OR together, how should the SOF-IRQs be configured? Only on one device and hope that the clock synchronization regards all devices and all channels?

How do I make sure that I get no PWM-artifacts?

Many thanks & Best Regards

Gerardo

0 REPLIES 0