2024-12-13 12:33 AM
Dear Community,
using the STEVAL-ILL089V1 board we would like to power a string of 12 LEDs (Cree XLamp Element G LED Data sheet) and use the PWM dimming function. While the respective raising and falling DIM treshold voltages are clearly stated in the ALED6000 datasheet, I am not sure about the practicable PWM input frequency and resolution. As I am not that experienced in the electronics field yet, I would highly appreciate if you could give me recommendations for the PWM input frequency and practicable resolution (minimal increment / step size).
Thanks in advance and best regards,
Ingmar
Solved! Go to Solution.
2024-12-14 1:19 AM
Hi,
The limits are in the data sheet, so you can choose...
Usually basic driving frequency is > 100 Hz, to avoid visible flickering. But on LEDs you might still see some flickering, so I would recommend a frequency about 2khz to start with.
Then question is: what you want to do with it?
Need a very wide range for dimming?
Our eyes get the impression of brightness almost on a logarithmic scale, so reducing the pwm from 100% to 90% changes almost nothing in brightness. To get it to visible low light levels, you need to go to 1% pwm or lower.
So maybe useful to have a pwm with 1024 ticks and dimming is just always half or double the pwm width, from min to max.
Just try it to see, how it looks. Then you know.
2024-12-14 1:19 AM
Hi,
The limits are in the data sheet, so you can choose...
Usually basic driving frequency is > 100 Hz, to avoid visible flickering. But on LEDs you might still see some flickering, so I would recommend a frequency about 2khz to start with.
Then question is: what you want to do with it?
Need a very wide range for dimming?
Our eyes get the impression of brightness almost on a logarithmic scale, so reducing the pwm from 100% to 90% changes almost nothing in brightness. To get it to visible low light levels, you need to go to 1% pwm or lower.
So maybe useful to have a pwm with 1024 ticks and dimming is just always half or double the pwm width, from min to max.
Just try it to see, how it looks. Then you know.