cancel
Showing results for 
Search instead for 
Did you mean: 

Precision voltage reference with low 1/f noise

Tommino
Senior

Hi all,

 

I am looking for two voltage references to produce two rails ( positive and negative) with low frequency noise.

The voltage reference does not need to have a tight output voltage accuracy and long term precision. It needs to be stable over a 1minute period and this is why I am looking for low 1/f noise.

The application is shown in this circuit and I need to get these two references to supply the voltage divider. So far I was supplying the divider with the same +/-5V used for the amplifiers and taken from two linear voltage  regulators ( L78L05ACUTR for the +5V L79L05ACUTR for the -5V): with this setup I get too much noise at the output of the second amplifier which can amplify up to a factor x57.  This noise is not coming from the opamp ( is a low noise opamp from a competitor OPA4205) or the input at pin3 which has been already proven to be noise-free.

 

Immagine 2025-02-05 123152.jpg

 Can you recommend a couple of possible IC to produce two stable references from the +/-5V already present in the circuit? Ideally the ICs should have fixed output at 3 or 4V and be low-cost. The 1/f integrated noise over 0.1Hz-10Hz as low as possible.

 

Best regards

4 REPLIES 4
Uwe Bonnes
Principal III

78xx is not meant for low noise. Look for low noise regulators. B.t.w., there is no "noise-free", there is only (ultra) low noise.

Hi Uwe,

Sure I meant "noise-free" for my application :)

Do you know pin to pin replacement of

"L78L05ACUTR for the +5V L79L05ACUTR for the -5V"

for low-noise regulators?

Uwe Bonnes
Principal III

Ask a search engine first, or look on the ST. TI. Analog Devices, etc web page.

Tommino
Senior

Ok sure. I would like also to wait for some other comment from ST engineers