cancel
Showing results for 
Search instead for 
Did you mean: 

Powering usb-c device with power supply that doesn't support PD

trivettegiacomo
Associate

Hi, i'm trying to power an usb-c device that needs 5v 2A, with a power supply (5v 8A) that doesn't support power delivery. For doing that i tried to use the evaluation board EVAL-SCS002V1 connecting the power supply wires (+ and -) to the green connector and the usb-c one to the device to power on. The result is that only the board blu led is turning on that means "default USB current".

How can i negotiate for more current? What am i doing wrong?

Please help me 🙏.

Regards,

Giacomo

1 ACCEPTED SOLUTION

Accepted Solutions
willzhou
ST Employee

Hi

Please check this doc, it need to modify some register.

pm0265-managing-usbc-port-status-with-the-stusb4500l--stmicroelectronics.pdf

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
willzhou
ST Employee

Hi

Please check this doc, it need to modify some register.

pm0265-managing-usbc-port-status-with-the-stusb4500l--stmicroelectronics.pdf

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.