2025-01-11 11:36 PM
hi ,
Aiming to have few minutes power back up for STM32 mcu with SD card incase main supply 5v goes OFF condition . Timer added for capacitor charging time since initial current is will be little high .
The above is setup enough ? or something special circuit to be build for super capacitor ?
2025-01-12 02:23 AM
Normally this Supercap's have rather high ESR, so probably not a good idea. If You really need some minutes of backup you will need to do this with a battery, If you need only some 100's of ms then I would use some "normal" Capacitor, but be award that the STMPS2151 will only work down to about Vout + 0.5V.
2025-01-12 04:01 AM - edited 2025-01-12 04:10 AM
hi,
can you suggest 3.7v battery charger + battery switch over to main supply handling IC number ?.