cancel
Showing results for 
Search instead for 
Did you mean: 

PC based GUIs to operate dspin HW

scope
Associate II
Posted on January 08, 2015 at 20:54

There is no useful information on the ST website (none I can find in three days) that explains which PC GUIs can be used with which eval systems. Can someone explain which PC GUIs are avaliable for which Eval systems and what functions they implement?

The ST website has much information on the HW, but none on the SW except links to download, but so far, none of them will launch without the EVAL board connected, so I cant even see screen shots except for the PractiSpin, but I dont know what HW that works with.

AN1794 discusses PractiSpin, but I cannot find a similar discussion of c or dSPIN and cannot order harware until I know what the GUI does.

Various documents for the dSPIN HW refer to ''available GUI'' but no links or discussion of what that is.
1 REPLY 1
Gigi
ST Employee
Posted on January 09, 2015 at 08:43

Ciao David

The forum to discuss about xxxSpin family is this:

https://my.st.com/public/STe2ecommunities/motordriver_ics/Lists/Motor%20Driver%20ICs%20and%20Boards

Ciao

Gigi