2023-10-16 09:55 PM
Can i know the minimum Operating temperature range of this IC "STW4N150"
Solved! Go to Solution.
2023-10-18 06:01 AM - edited 2023-10-18 06:02 AM
Please note that the storage temperature must not be confused with the operating temperature and only refers to the storage of the device.
There is nothing to prevent operation at -30°C if the applicable parameters of the data sheet are observed.
2023-10-17 12:45 AM
Welcome @Pradeep2014, to the community!
you can use the STW4N150 down to -40°C, the data sheet also shows some graphs for -50°C.
Hope that helps?
Regards
/Peter
2023-10-17 02:52 AM
2023-10-18 06:01 AM - edited 2023-10-18 06:02 AM
Please note that the storage temperature must not be confused with the operating temperature and only refers to the storage of the device.
There is nothing to prevent operation at -30°C if the applicable parameters of the data sheet are observed.