2016-08-30 10:21 AM
Hi.
I designed the power converter which is supply from the photovoltaic cell ( Umax = 5.5 V / 1 W) on a SPV1040. The problem is that the system did not stabilize the output voltage.The output voltage is proportional to the input voltage. I attach the schematic: Someone sees what mistake I make?2016-08-30 10:43 AM
I forgot to add that I no soldering diodes D1 and
D2. :)