2024-04-24 10:58 PM - last edited on 2024-04-25 2:54 AM by Peter BENSCH
Respected Sir/Ma'am,
I'm designing 2KW SMPS from reference schematics design of "STEVAL-ISA172V2: 2 KW fully digital AC-DC power supply (D-SMPS) evaluation board". I've not faced any obstacle in designing schematics of the circuit with help of reference design. But in PCB design, I'm facing so much problem in Altium Design Professional Software.
I'll be grateful to you if you'll share the CAD/CAE symbol, Gerber file, PCB layout, Assembly drawing of "STEVAL-ISA172V2" with me so that I can complete this design for physical board implementation. It will be very helpful for me to complete my project. I'm waiting for your reply.
Thanks & Regards,
Solved! Go to Solution.
2024-04-25 2:58 AM
Welcome @Arghya_FPGA, to the community!
The GERBER data can be found alongside the BOM and the schematics on the product website under the tab CAD Resources. As the board was launched many years ago, it is possible that no Altium data is available.
Hope that helps?
Regards
/Peter
2024-04-25 2:58 AM
Welcome @Arghya_FPGA, to the community!
The GERBER data can be found alongside the BOM and the schematics on the product website under the tab CAD Resources. As the board was launched many years ago, it is possible that no Altium data is available.
Hope that helps?
Regards
/Peter
2024-04-25 5:30 AM
2024-04-25 5:57 AM
As already mentioned, the circuit diagrams can also be found on that website. The PCB layout is only available in GERBER format.
2024-04-26 12:18 AM
Respected Sir,
Thanks you so much for your reply & concern. I'm really grateful to you.
Thanks & Regards.
2024-05-06 12:28 AM
Respected Sir,
In STEVAL-ISA172V2 schematics design there are two STM32F33C8T6 as primary & secondary MCU. My query is to you that when we want to implement these two ICs in assembly of PCB, is there any programming have to do for these ICs or not?
And if there would be some programming for this, how could I do by myself? What would be the procedure for programming, please let me know.
I'm eagerly waiting for your reply.
Thanks & Regards.
2024-05-06 1:01 AM
The MCUs must of course be programmed. The project for a 2kW converter is a little too complex to be discussed here in the community. If you cannot do this yourself, you should contact your local power expert or your distributor.