2024-10-07 10:49 AM
We've been using the On Semi FDD8453LZ MOSFET (40V, 6.7 ohm, DPAK) in our motor control designs for many years, but this part is now EOL. We're looking for a suitable DPAK replacement. One critical parameter is the single pulse avalanche energy, which must be equal or better than the FDD8453LZ's 253 mJ. Unfortunately this is not a parameter that normally is listed in parametric selection tables. Does ST have a 40V DPAK MOSFET that meets this requirement?
Thanks,
Mark
2024-10-07 02:52 PM
Welcome @WiscEng, to the community!
what about e.g. the STD120N4F6 with 394mJ in DPAK?
Regards
/Pete