cancel
Showing results for 
Search instead for 
Did you mean: 

Need DPAK MOSFET with high avalanche rating

WiscEng
Visitor

We've been using the On Semi FDD8453LZ MOSFET (40V, 6.7 ohm, DPAK) in our motor control designs for many years, but this part is now EOL.  We're looking for a suitable DPAK replacement.  One critical parameter is the single pulse avalanche energy, which must be equal or better than the FDD8453LZ's 253 mJ.  Unfortunately this is not a parameter that normally is listed in parametric selection tables.  Does ST have a 40V DPAK MOSFET that meets this requirement?

Thanks,

Mark 

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @WiscEng, to the community!

what about e.g. the STD120N4F6 with 394mJ in DPAK?

Regards
/Pete

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.