2006-01-31 10:29 PM
MTIM and related MPRSR???
2011-05-17 01:19 AM
Hi.
I have some problems in understanding by control the MPRSR ratio bits. I found also the thread http://mcu.st.com/mcu/modules.php?mop=modload&name=Splatt_Forums&file=viewtopic&topic=2696&forum=13 But it is not clear enough for me. So, where exactly occur the step frequency and why is the minimum value for MTIM is 55h? I try to drive a BLDC motor with the ST7FMC so lets check a example: F_Periph = 4 MHz and the MPRSR Reg is loaded by 8h and the uC works in switched mode. So, that means the MTIM works at a clock of 7,8125kHz. Now it takes 19.2ms for next C event then MCOMP comprised 150. MTIM timer is reset and 'ratio' bits will be kept at 8h. Is this right? Maybe it is not a smart question but it is a new field for me. Thanks for help, By RoB.2011-05-17 01:19 AM
Hi,
the management of ratio value for MTIM timer depends on the mode the MCU is configured: Switched or Auto-switched. The mechanism can be easily understood just before reading carefully the at pages 168->173. In this way, I believe that all your questions can be completely answered. If not, please, let me know further at this location. Best regards, Tanio