2019-11-05 06:40 AM
Required PWM - 16 Channel for the motor controller application .please suggest the best MCU with support RTOS.
2019-11-05 07:58 AM
How many different frequencies concurrently?
2019-11-06 03:43 AM
from 16khz to 30khz or more .... in one MCU we have to run 5 motor so we required more PWM channel.
In addition we have to build the application in RTOS so good support of RTOS lib and SDK also required from STM.
2019-11-06 03:43 AM
16khz to 30khz is PWM frequency.
2019-11-06 06:03 AM
from 16khz to 30khz PWM Frequency or more .... in one MCU we have to run 5 motor so we required more PWM channel.
In addition we have to build the application in RTOS so good support of RTOS lib and SDK also required from STM.
2019-11-06 09:29 PM
can any body suggest the MCU for motor controller application with 16 or more PWM ,with RTOS support