cancel
Showing results for 
Search instead for 
Did you mean: 

L6982CDR application problem.

PL3
Associate II

Hi,We're encountering an issue with the L6982CDR buck converter in our application. Here's the detailed scenario: Configuation: We're using it to convert a 24V input to a 5V output to power the board. Load: The 5V output supplies a load current of approximately 200mA. System Context: The same 24V input is also used to drive a stepper motor. Problem:Following mass production, some units have experienced a loss of the 5V output. The occurrence rate of this failure is low. Key Observations: This fault occurs during operation, not at power-up. The fault clears if the 24V power is restarted. When the failure happens, we measured a normal 24V input voltage and a normal voltage at the VCC pin of the IC. However, the SW pin output remains low. Notably, we have used this chip reliably for a long time, and this is a recent issue.

Here is the schematic of our product:

PL3_1-1760668895581.png

 

Here is the PCB of our product:

PL3_0-1760668869816.png

 

Please let me know if anything is unclear or if you need any tests performed We would appreciate your guidance on troubleshooting this.

12 REPLIES 12
Wtm
Associate II

Hi @teba99 

We still haven't identified the root cause. The probability of reproducing the fault is too low. For the new version, we have thickened the VCC pin routing. The 26 test samples have aged for a month, but no faults have occurred yet.

Could you please share the layout and routing of your PCB?

teba99
Associate II

Hi @Wtm ,

Thanks for the reply. Let me get back to you.

Hi @Wtm ,

We've gotten some pointers and are investigating ESD/noise/spikes/levels on the EN and SW as possible triggers for the internal oscillator to stop or fail to restart. We'll loop back once we know more. Thanks!