2013-03-06 7:20 AM
I am trying to get the L6480 Demo board communicating with the L6480 Evaluation software using the the STEVAL-PCC009V2. I have tried in Windows 7 and Windows XP and was able to get the driver for the PCC0009V2 loaded on both O/Ss. However, I have not had any success communicating to the L6480. There is a comment that the PCC009V2 needs a firmware update, but I cannot find the firmware update tool IBUUI or the firmware to update the board.
2013-03-12 3:24 AM
Hi,
did you tried the ?This is a the last Win7 application for the evaluation of the dSPIN and cSPIN family products and it includes also a firmware update for the PCC009V2.RegardsEnrico2013-03-15 10:56 AM
Yes it turned out to be a problem with my PCC0009V2 board. Once that was replaced it is working fine. Thanks.