2014-10-02 1:29 PM
I am attempting to run the L6470H discovery kit with the dspin software from a machine with windows xp on it. I was previously able to run it from another machine with xp, I installed the same files but cannot connect to the board. I get a windows error with the following parameters:
EventType : clr20r3 P1 : gui.exe P2 : 1.2.5071.18356 P3 : 528b2b58 P4 : mscorlib P5 : 2.0.0.0 P6 : 4a7ce2b8 P7 : 1295 P8 : 14 P9 : system.missingmethodexception On the other system I get an error with spi_dll when I connect, any ideas? I have tried to download the latest software with no luck. #l6470h #discovery-eval6470-disc2014-10-03 7:03 AM
Hi,
The SPINFamily software is based on the Microsoft .NET framework. Please, check the installation of this component. Regards Enrico2014-10-03 9:21 AM
I installed 4.0 and I get the same error, this time it is delayed by a few minutes. do I need to install a different version of .net?