cancel
Showing results for 
Search instead for 
Did you mean: 

L6207

apoggiali
Associate II
Posted on September 07, 2011 at 10:11

Hi gentlemen

I'm planning to use L6207 PD for 2 brushed D.C motors, does any body know whether is it possible to use n.c. pins close the outputs to increase the path's width or they must be left unconnected.

I'm quite surprise only one pin is used to deliver 2.8 RMS Amps, and data sheet is'nt so clear about that.

Thanks for suggestions
2 REPLIES 2
bille.stello
Associate III
Posted on September 09, 2011 at 09:05

Hello,

the 2.8Arms are indeed guaranteed from only one pin. About the n.c. pins,  it's a good idea to connect them to ground plane so as to facilitate heat dissipation.

Regards,

Billino

apoggiali
Associate II
Posted on September 09, 2011 at 11:21

Thanks a lot Billino for your usefull help.

Alf