cancel
Showing results for 
Search instead for 
Did you mean: 

L6207 PWM Current Control Question

dstetson
Associate
Posted on July 30, 2014 at 19:04

Could someone please explain how current is controlled on the L6207 via onboard PWM Current Controller?  Additionally, AN1762 APPLICATION NOTE indicated a constant current could be obtained through a simple voltage divider into Vref.  

For example, I want to cap the current at 1.5A / phase, what type of PWM or voltage division would I need to implement? 

Thank you.

#l6207
1 REPLY 1
Enrico Poli
ST Employee
Posted on August 21, 2014 at 14:29

Hello,

the current level is set according to the following formula:

Iphase = Vref/Rsense

where Vref is the reference voltage you set at the REF input and Rsense is the shunt resistor connected between the SENSE pin and ground.

Regards

Enrico