2024-11-29 8:55 PM
Is there any tolerance spec available for I_PU (the 20uA pull-up current on the outputs) of the IPS4260L?
Solved! Go to Solution.
2024-11-30 11:13 AM
Ipu is a simple internal constant current source for which the usual semiconductor tolerances can be assumed, i.e. in the region of approx. 40%. However, there is no publicly documented and therefore guaranteed specification for this.
Does that help you?
Regards
/Peter
2024-11-30 11:13 AM
Ipu is a simple internal constant current source for which the usual semiconductor tolerances can be assumed, i.e. in the region of approx. 40%. However, there is no publicly documented and therefore guaranteed specification for this.
Does that help you?
Regards
/Peter
2024-11-30 5:25 PM
That helps. I assume it's not possible to disable this feature?
2024-12-01 1:25 AM
Correct, the feature Ipu cannot be disabled.