2019-11-18 4:59 AM
as per the figure we provides a dc voltage as a input to the interleaved active clamp flyback converter block, provide a PWM signal to the MOSFET which is in interleaved block for switching purpose. PWM signal is generated by the microcontroller which has a fix frequency 57 KHz and 50 % duty cycle then we got a output like triangular waveform. actually we will need a output like a given figure so which type of PWM output will be provided to the switching MOSFET, so we got proper output of the interleaved active clamp flyback converter.