cancel
Showing results for 
Search instead for 
Did you mean: 

Identify this Component

Raj3
Associate II

Good morning sir 

Pls identify the component.i don't understand 

1 REPLY 1
Peter BENSCH
ST Employee

It's the obsolete fast recovery diode SMBYT03-400 in package SMC:

  • VRRM=400V
  • IFav=3A
  • IR<10µA @25°C, <600µA @100°C
  • trr<25ns

You could consider the STTH3R04S as a replacement.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.