cancel
Showing results for 
Search instead for 
Did you mean: 

I need to replace an old L5991A. The question is which L5991XXX is drop-in replaceable? L5591AD?

AAnde.5
Associate
 
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @AAnde.5​, to the community!

Even if the L5991 is old, only the DIP16 package is obsolete, the SO16 package is still in production, so I moved your question from Discontinued Products to Power Management.

Yes, it would be a good idea to switch to the L5991AD.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @AAnde.5​, to the community!

Even if the L5991 is old, only the DIP16 package is obsolete, the SO16 package is still in production, so I moved your question from Discontinued Products to Power Management.

Yes, it would be a good idea to switch to the L5991AD.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.