cancel
Showing results for 
Search instead for 
Did you mean: 

Hola, necesito diseñar un VFD, Driver Variador de Frecuencia, me pueden apoyar, que tipo de módulos necesito para el diseño IGBT, fuente de Voltaje , Micro-controlador, driVer, etc. Para motor TRIFASICO información por favor

CPere.2
Associate
 
2 REPLIES 2
Javier1
Principal

Hola @CPere.2​ , aqui la gente funciona en inglés.

Para que te puedan ayudar mejor yo que tu traduciria al inglés tu pregunta.

También deberias poner un titulo corto y hacer tu pregunta en el cuerpo del post.

saludos!

we dont need to firmware by ourselves, lets talk
Cristiana SCARAMEL
ST Employee

Hello @CPere.2​ and welcome to the ST Community.

I translate you question with Google translator:

Hello, I need to design a VFD, Variable Frequency Driver, Can you support me, what kind of modules do I need for the design?

IGBT, Voltage source, Micro-controller, driVer, etc. For THREE-PHASE motor information please

The first step is identify the application ratings in terms of supply voltage and motor current according to your motor part number.

Then we can try to identify the best solution fitting your application requirements (MCU, drivers, power stage and so on).

For a better support, feel free to share more details on your application.

If you feel a post has answered your question, please click "Accept as Solution"