2022-09-12 6:36 AM
2022-09-12 6:48 AM
Welcome, @_Sansindhu, to the community!
STEF01 can drive an external FET, but it is in series and only serves to protect against polarity reversal. Since the STEF01 is connected to the full input voltage, but is destroyed above 55V, it cannot work with your 145V.
By the way, all our e-fuses currently work up to a maximum of 55V, so we cannot yet recommend a possible solution.
Does it answer your question?
Regards,
/Peter
2022-09-15 10:28 PM
Thanks Peter!
2022-09-19 12:49 AM
Your're welcome!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter