2021-07-19 10:49 PM
I am using 12V motor, all the phase I measured 12V, its look like it stuck at brake.
what can be the problem?
I am using motor 1028m012b - FAULHABER
Solved! Go to Solution.
2021-07-20 07:37 AM
I confirm that the only configuration that brings all outputs high is the brake function.
Try to verify the voltage as close as possible to the BRAKE pin (#20), if is correctly set high.
2021-07-20 11:27 PM
I checked pin 20 =5V.
also checked pin 19 and i found that Vref is 0V,
the problem with the evaluation board, I connected J6 2-3 and J3-11 to 5V, and no vref voltage.
still the motor not moving, but now I see current consumption from my power supply.
2021-07-20 11:58 PM
I measured PIN 20 BRAKE = 5V
checked PIN 19 VREF = 0V
the problem is with evaluation board I connected J6 2-3 and powered J3-11 with 5V and no voltage to VREF.
now I powered the VREF and I see power consumption but still the motor not moving.
2021-07-20 11:59 PM
The schematic of the evaluation board is not correct.
2021-07-21 12:42 AM
The motor at the power up try to move but not moving (feel vibration at the start).
the HALL EFFECT H1=0 H2=1 H3=0 not changing.
2021-07-21 02:20 AM
Hi @IGAL TALOR for easier reading, please try to concentrate the information in a single post.
Where you are applying the VREF voltage instead of J3-11?
Are you applying the 5V to the J3-1 pole?
If you identify a mismatch between board and schematic please share the information, thanks.
2021-07-21 02:33 AM
the VREF from J3-11 is not connected as shown at the schematic, I checked it with FLUKE.
now I connected VREF from J8-3.
Do you know about another mismatches?
2021-07-22 12:49 AM
Hi @IGAL TALOR,
I checked the board connection: the silkscreen of J6 solder bridge is swapped compared to the schematic.
The right info for VREF source selection is reported in the figure 1 of data brief .
If the issue persist I suggest to check all the IC pin status with a oscilloscope probe (not multimeter).
2021-07-29 06:41 AM
Hi @IGAL TALOR ,
are there any updated about your project progress?
2021-07-31 11:12 PM
HI,
I am waiting for a new motor that I ordered.
I think that the motor that I used was damaged.
the hall effect not changing.