cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I am new to a project with the STEVAL-SPIN 3201. If I connect the board via USB it doesn't appear as a disk. Is there a way to reset the board, to setup it up again? Thanks!

MRauc.1
Associate
 
2 REPLIES 2
Cristiana SCARAMEL
ST Employee

Hello @MRauc.1​ and welcome to the ST Community.

What do you mean, it doesn’t appear as disk? 

The "SPIN32F0" it is not listed in the "Devices and drives" of your PC?

In this case could be a driver issue, I suggest to install the STSW-LINK009

In any case to be able to program the STSPIN32F0 you need to power the board (J2 connector).

Let me know if this info is useful to you, if yes please "Select as Best" button to close the topic.

If you feel a post has answered your question, please click "Accept as Solution"

Hello @MRauc.1​,

any news about your issue?

If you feel a post has answered your question, please click "Accept as Solution"