cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, Could you give some information regarding this component, Part No : LD1117S50TR Can you give information regarding pin dimension marked with X (refer image) Thank you

aadza.1
Associate
 
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @aadza.1​, to the community!

We would like to apologize that this information was not taken over from the standard JEDEC TO-261: the value X and Y in your drawing is called L by JEDEC and the value min 0.75mm is given, typical and max values do not exist for this value.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.