2022-02-25 03:26 PM
I am trying to identify a transient voltage suppressor manufactured by ST that I need to replace.
I have not been able to determine the correct product based on the coding found on the package. Would anyone here be able to identify this TVS?
The coding appears to be C3J C616, but it is a bit unclear. The package is a surface mount approx. 3mm x 5mm. The TVS is used in a 24V pool actuator valve control system.
Solved! Go to Solution.
2022-02-27 06:52 AM
C616 is likely a production code
CBJ is SMBJ40CA
https://www.st.com/resource/en/datasheet/smbj.pdf
2022-02-27 06:52 AM
C616 is likely a production code
CBJ is SMBJ40CA
https://www.st.com/resource/en/datasheet/smbj.pdf
2022-02-27 08:27 PM
Thanks!
2023-08-18 09:35 AM
I cannot seem to find any information on one with a case code of L35. It is across the 24v windings of a transformer.
2023-08-18 12:26 PM
@KI0HA Well, your question is a new topic, for which you should actually open a new thread. Anyway, the component with L35 could be e.g. the so-called Trisil SMP100LC-35, but of course also a completely different one. Without a good recognizable photo you can only guess.
Regards
/Peter