cancel
Showing results for 
Search instead for 
Did you mean: 

Help to identify a TVS?

PeterB1
Associate

I am trying to identify a transient voltage suppressor manufactured by ST that I need to replace.

I have not been able to determine the correct product based on the coding found on the package. Would anyone here be able to identify this TVS?

The coding appears to be C3J C616, but it is a bit unclear. The package is a surface mount approx. 3mm x 5mm. The TVS is used in a 24V pool actuator valve control system.

1 ACCEPTED SOLUTION

Accepted Solutions

C616 is likely a production code

CBJ is SMBJ40CA

https://www.st.com/resource/en/datasheet/smbj.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

4 REPLIES 4

C616 is likely a production code

CBJ is SMBJ40CA

https://www.st.com/resource/en/datasheet/smbj.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks!

I cannot seem to find any information on one with a case code of L35. It is across the 24v windings of a transformer.

@KI0HA Well, your question is a new topic, for which you should actually open a new thread. Anyway, the component with L35 could be e.g. the so-called Trisil SMP100LC-35, but of course also a completely different one. Without a good recognizable photo you can only guess.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.