cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, Is it Ok to use VNH5180A-E Vcc power value 30V (Abs max is 41V and Op supply voltage max is 18V) ?

KRönn.1
Associate

VNH5180A-E

1 REPLY 1
Peter BENSCH
ST Employee

The VNH5180A-E is an automotive device, so it must withstand/survive test pulses at the supply line, which are defined in ISO 7637-2:2004(E), see the datasheet, pg 16. There is a built-in overvoltage clamp to fulfil these requirements.

So, it is not OK to run the VNH5180A-E permantely with 30V. The recommended operating conditions can be found in the datasheet pg. 9 under Electrical characteristics, giving for Vcc=5.5...18V.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.