2019-09-11 08:02 AM
On opening the STPM34 eval software and connecting USB to UART to PC.
Under Option>Interface> Communication, I selected Port type as USB and tried to open port.
Error window pop up - 'unhandled exception has occurred' as shown in Fig. 2.
This error remains even if I remove USB to UART from PC.
Error window: Also, check error details in attached notepad file.
Even after that I continued and selected USB port and open.
'Failed opening IO lib' window pop up as shown in Fig. 3.
Please give me suggestions.
System details:
Model : Lenovo Win7 PC 64 bit
OS : Window 10 Home
Software installed from ST link web site.
Also, installed Virtual COM drivers.
2019-09-13 06:40 AM
I tried on Windows 7. Its working finely.
Is there any window requirement for handling Eval software?
On Window 10, its showing error continuously.
2019-10-16 04:57 AM
@Madhura C I'm using STMP33/34 eval board for my project. and I'm using Windows10 Pro , Works fine.
I think You should select the proper Interface and give separate power to the interface (Isolated 3.3V Supply).