Skip to main content
Lead
January 28, 2026
Solved

What Device Tree/Configuration of USART/UART does the MP2xROMtracesdump have?

  • January 28, 2026
  • 8 replies
  • 613 views

I have built a custom board by using STM32MP257F and I want to boot on USART6. 

I have not succeed to boot on USART6 when I compile my own fsbla by change the device tree of TF-A.

I got a suggestion from ST Dev team to run this ROM tracedump wiki-stm32mp-addons/MP2RomTracesDump at 6.1.0 · STMicroelectronics/wiki-stm32mp-addons · GitHub and it gave me a positive output on USART6. 

The soldering was OK. The BootROM was OK and the UART6 was alive. This is the output from my USART6.

===================================================
== STM32MP25 cut2.x bootrom display traces V1.01 ==
== Date of compilation : Jun 26 2024 - 11:25:23 ==
===================================================
Executed on Cortex A35 - Aarch64
Successfully booted on interface SD instance 1
Reset reason : POR reset
Chip state : CLOSED_UNLOCKED
==================================================================
Bootrom traces
==================================================================

[INFO] - BOOTCORE_FreezeIWDG12Clocks >
[INFO] - BOOTCORE_HwResetPOR >
[INFO] - BOOTCORE_VarLastValidAppRstMask ( 0x00000015 ) >
[INFO] - BOOTCORE_VarLastValidCpu1RstMask ( 0x00000003 ) >
[INFO] - BOOTCORE_VarLastValidPwrResetSource ( 0x00000000 ) >
[INFO] - BOOTCORE_ValRegHwRstSclrr ( 0x00000000 ) >
[INFO] - BOOTCORE_ValRegC1HwRstSclrr ( 0x00000000 ) >
[INFO] - BOOTCORE_ValRegC1BootRstSclrr ( 0x00002035 ) >
[INFO] - BOOTCORE_ChipModeClosedUnlocked >
[INFO] - BOOTCORE_LogicalResetSystem >
[INFO] - BOOTCORE_BootActionSecureBootProcess >
[INFO] - BOOTCORE_BootPinsSrcSel ( 0x00000001 ) >
[INFO] - BOOTCORE_BootCfgOtpWordValue ( 0x00000000, 0x00000000, 0x00000000 ) >
[INFO] - BOOTCORE_OtpBootpinLayoutSrc ( 0x00000000 ) >
[INFO] - BOOTCORE_OtpSrcSel ( 0x00000000 ) >
[INFO] - BOOTCORE_BootSrcIndexByBootPins ( 0x00000001 ) >
[INFO] - BOOTCORE_BootSrcIndex ( 0x00000001 ) >
[INFO] - BOOTCORE_SRCSEL_A35_SDCARD_SDMMC1_SDCARD_SDMMC1 >
[INFO] - BOOTCORE_OtpBootSrcDisableMaskVal ( 0x00000000 ) >
[INFO] - BOOTCORE_OtpBootUartInstanceDisableMaskVal ( 0x00000000 ) >
[INFO] - CSPID_CSPDEVICE ( 0x00000003 ) >
[INFO] - BOOTCORE_BootCfgAfmuxOtpWord1Value ( 0x00000000 ) >
[INFO] - BOOTCORE_BootCfgAfmuxOtpWord2Value ( 0x00000000 ) >
[INFO] - BOOTCORE_BootCfgAfmuxOtpWord3Value ( 0x00000000 ) >
[INFO] - BOOTCORE_BootCfgHseValue ( 0x00000000 ) >
[INFO] - BOOTCORE_EnabledSrcMaskVal ( 0x00000688 ) >
[INFO] - BOOTCORE_BootCfgHseValue ( 0x00000000 ) >
[INFO] - BOOTCORE_WDGStartAndUnfreeze >
[INFO] - BOOTCORE_UnFreezeIWDG12Clocks >
[INFO] - BOOTCORE_BootModeSECUREBOOT >
[INFO] - BOOTCORE_SecureBootLoadFsblA >
[INFO] - BOOTCORE_StartupWaitTime >
[INFO] - BOOTCORE_Pll14StartBegin >
[INFO] - BOOTCORE_NoCpuPllOtpBitValue ( 0x00000000 ) >
[INFO] - BOOTCORE_Pll1Locked >
[INFO] - BOOTCORE_CkMpuSwitchedOnPll1 >
[INFO] - BOOTCORE_Pll4Locked >
[INFO] - BOOTCORE_CkAxiSwitchedOnPll4 >
[INFO] - FLASHBOOT_HandleInit ( 0x00000003 ) >
[INFO] - SD_CardDetected >
[INFO] - SD_HighCapacityCardSDHCOrSDXC >
[INFO] - SD_TryFSBL1 >
[INFO] - SD_GPTFound >
[INFO] - SD_FsblsFound ( 0x00004400, 0x00044400 ) >
[INFO] - DWNLDMGR_FoundPaddingHeader >
[INFO] - SECBOOTCUSTOM_EnableDataCache >
[INFO] - SECBOOT_AuthenticationExtensionHeaderMissing >
[INFO] - SECBOOT_AuthImageLength ( 0x0000E400 ) >
[INFO] - SECBOOT_AuthImageEntryPoint ( 0x0E002600 ) >
[INFO] - SECBOOT_AuthDecisionIsJumpToImage >
[INFO] - SECBOOTCUSTOM_DisableDataCache >
[INFO] - BOOTCORE_AARCH64BootReq >
==================================================================

Question:

I'm planning to use USART6 as early debugging but I need to know what settings the ROMtracedump had for displaying and using USART6.

My Device Tree for TF-A have this following setting. But still, this won't work. I don't know why it won't work. Perhaps if I could know the settings fom the ROMtracedump, then I could understand why the USART6 is working as early debugging and not for my Device Tree for TF-A.

// SPDX-License-Identifier: (GPL-2.0-only OR BSD-3-Clause)
/*
 * Copyright (C) 2026, STMicroelectronics - All Rights Reserved
 * Author: STM32CubeMX code generation for STMicroelectronics.
 */

/* For more information on Device Tree configuration, please refer to
 * https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
 */

/dts-v1/;

#include <dt-bindings/pinctrl/stm32-pinfunc.h>
#include <dt-bindings/clock/stm32mp25-clksrc.h>
*#include "stm32mp25-mx.dtsi"*

#include "stm32mp257.dtsi"
#include "stm32mp25xf.dtsi"
#include "stm32mp257f-firmware-mx-rcc.dtsi"
#include "stm32mp25xxak-pinctrl.dtsi"
#include "stm32mp25-ddr.dtsi"

/* USER CODE BEGIN includes */
/* USER CODE END includes */

/ {
	model = "STMicroelectronics custom STM32CubeMX board - openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11";
	compatible = "st,stm32mp257f-firmware-mx", "st,stm32mp257";

	memory@80000000 {
		device_type = "memory";
		reg = <0x0 0x80000000 0x00000001 0x00000000>;

		/* USER CODE BEGIN memory */
		/* USER CODE END memory */
	};

	/* USER CODE BEGIN root */
	
	aliases{
		serial0 = &usart6;
	};

	chosen{
		stdout-path = "serial0:115200n8";
	};

	clocks {
		clk_hse: clk-hse {
			#clock-cells = <0>;
			compatible = "fixed-clock";
			clock-frequency = <24000000>;
		};
	};
	
	/* USER CODE END root */

}; /*root*/

&pinctrl {
	i2c7_pins_mx: i2c7_mx-0 {
		pins {
			pinmux = <STM32_PINMUX('D', 14, AF10)>, /* I2C7_SDA */
					 <STM32_PINMUX('D', 15, AF10)>; /* I2C7_SCL */
			bias-disable;
			drive-open-drain;
			slew-rate = <0>;
		};
	};

	sdmmc1_pins_mx: sdmmc1_mx-0 {
		pins1 {
			pinmux = <STM32_PINMUX('E', 0, AF10)>, /* SDMMC1_D2 */
					 <STM32_PINMUX('E', 1, AF10)>, /* SDMMC1_D3 */
					 <STM32_PINMUX('E', 2, AF10)>, /* SDMMC1_CMD */
					 <STM32_PINMUX('E', 4, AF10)>, /* SDMMC1_D0 */
					 <STM32_PINMUX('E', 5, AF10)>; /* SDMMC1_D1 */
			bias-disable;
			drive-push-pull;
			slew-rate = <1>;
		};
		pins2 {
			pinmux = <STM32_PINMUX('E', 3, AF10)>; /* SDMMC1_CK */
			bias-disable;
			drive-push-pull;
			slew-rate = <3>;
		};
	};

	usart6_pins_mx: usart6_mx-0 {
		pins1 {
			pinmux = <STM32_PINMUX('F', 13, AF3)>; /* USART6_TX */
			bias-disable;
			drive-push-pull;
			slew-rate = <0>;
		};
		pins2 {
			pinmux = <STM32_PINMUX('F', 14, AF3)>; /* USART6_RX */
			bias-disable;
			drive-push-pull;
		};
	};

	/* USER CODE BEGIN pinctrl */
	/* USER CODE END pinctrl */
};

&pinctrl_z {
	/* USER CODE BEGIN pinctrl_z */
	/* USER CODE END pinctrl_z */
};

&bsec {
	status = "okay";

	/* USER CODE BEGIN bsec */
	board_id: board_id@3d8 {
		reg = <0x3d8 0x4>;
	};
	/* USER CODE END bsec */
};

&ddr {
	status = "okay";

	/* USER CODE BEGIN ddr */
	vdd1-supply = <&vdd1_ddr>;
	vdd2-supply = <&vdd2_ddr>;
	vddq-supply = <&vdd2_ddr>;
	/* USER CODE END ddr */
};

&hash {
	status = "disable";

	/* USER CODE BEGIN hash */
	/* USER CODE END hash */
};

&i2c7 {
	pinctrl-names = "default";
	pinctrl-0 = <&i2c7_pins_mx>;
	status = "okay";

	/* USER CODE BEGIN i2c7 */
	i2c-scl-rising-time-ns = <185>;
	i2c-scl-falling-time-ns = <20>;
	clock-frequency = <400000>;
	#address-cells = <1>;
	#size-cells = <0>;

	pmic2: stpmic@33 {
		compatible = "st,stpmic2";
		reg = <0x33>;
		status = "okay";

		regulators {
			compatible = "st,stpmic2-regulators";

			vddcpu: buck1 {
				regulator-name = "vddcpu";
				regulator-min-microvolt = <800000>;
				regulator-max-microvolt = <910000>;
				regulator-always-on;
			};
			vddcore: buck2 {
				regulator-name = "vddcore";
				regulator-min-microvolt = <820000>;
				regulator-max-microvolt = <820000>;
				regulator-always-on;
			};
			vddgpu: buck3 {
				regulator-name = "vddgpu";
				regulator-min-microvolt = <800000>;
				regulator-max-microvolt = <900000>;
				regulator-always-on;
			};
			vddio_pmic: buck4 {
				regulator-name = "vddio_pmic";
				regulator-min-microvolt = <3300000>;
				regulator-max-microvolt = <3300000>;
				regulator-always-on;
			};
			v1v8: buck5 {
				regulator-name = "v1v8";
				regulator-min-microvolt = <1800000>;
				regulator-max-microvolt = <1800000>;
				regulator-always-on;
			};
			vdd2_ddr: buck6 {
				regulator-name = "vdd2_ddr";
				regulator-min-microvolt = <1100000>;
				regulator-max-microvolt = <1100000>;
			};
			v3v3: buck7 {
				regulator-name = "v3v3";
				regulator-min-microvolt = <3300000>;
				regulator-max-microvolt = <3300000>;
				regulator-always-on;
			};
			vdda1v8_aon: ldo1 {
				regulator-name = "vdda1v8_aon";
				regulator-min-microvolt = <1800000>;
				regulator-max-microvolt = <1800000>;
				regulator-always-on;
			};
			vdd_emmc: ldo2 {
				regulator-name = "vdd_SD_card_temporary";
				regulator-min-microvolt = <3300000>;
				regulator-max-microvolt = <3300000>;
				regulator-always-on;
			};
			vdd1_ddr: ldo3 {
				regulator-name = "vdd1_ddr";
				regulator-min-microvolt = <1800000>;
				regulator-max-microvolt = <1800000>;
			};
			vdd3v3_usb: ldo4 {
				regulator-name = "vdd3v3_usb";
				regulator-min-microvolt = <3300000>;
				regulator-max-microvolt = <3300000>;
				regulator-always-on;
			};
			v5v_hdmi: ldo5 {
				regulator-name = "v5v_hdmi";
				regulator-min-microvolt = <2000000>;
				regulator-max-microvolt = <2000000>;
			};
			vdd_sdcard: ldo7 {
				regulator-name = "vdd_sdcard";
				regulator-min-microvolt = <3300000>;
				regulator-max-microvolt = <3300000>;
				regulator-always-on;
			};
			vddio_sdcard: ldo8 {
				regulator-name = "vddio_sdcard";
				st,regulator-bypass-microvolt = <3300000>;
				regulator-min-microvolt = <1800000>;
				regulator-max-microvolt = <3300000>;
				regulator-always-on;
			};
		};
	};
	/* USER CODE END i2c7 */
};

&iwdg1 {
	status = "disable";

	/* USER CODE BEGIN iwdg1 */
	timeout-sec = <32>;
	/* USER CODE END iwdg1 */
};

&pka {
	status = "disable";

	/* USER CODE BEGIN pka */
	/* USER CODE END pka */
};

&rcc {
	status = "okay";

	/* USER CODE BEGIN rcc */
	/* USER CODE END rcc */
};

&rng {
	status = "disable";

	/* USER CODE BEGIN rng */
	/* USER CODE END rng */
};

&saes {
	status = "disable";

	/* USER CODE BEGIN saes */
	/* USER CODE END saes */
};

&sdmmc1 {
	pinctrl-names = "default";
	pinctrl-0 = <&sdmmc1_pins_mx>;
	status = "okay";

	/* USER CODE BEGIN sdmmc1 */
	st,neg-edge;
	bus-width = <4>;
	vmmc-supply = <&vdd_sdcard>;
	vqmmc-supply = <&vddio1>;
	/delete-property/ cap-sd-highspeed;
	/delete-property/ cap-mmc-highspeed;
	/* USER CODE END sdmmc1 */
};

&usart6 {
	pinctrl-names = "default";
	pinctrl-0 = <&usart6_pins_mx>;
	status = "okay";

	/* USER CODE BEGIN usart6 */
	/* USER CODE END usart6 */
};

/* USER CODE BEGIN addons */
/* USER CODE END addons */

 

Best answer by PatrickF

Hi, 

MP2RomTracesDump is a bare-metal SW, not using Device Tree.

 

Have you looked in details this post ? 

https://community.st.com/t5/stm32-mpus-products-and-hardware/change-default-tf-a-and-u-boot-serial-linux-console/m-p/195027/highlight/true#M5675

 

Regards.

 

8 replies

PatrickF
PatrickFBest answer
ST Employee
January 29, 2026

Hi, 

MP2RomTracesDump is a bare-metal SW, not using Device Tree.

 

Have you looked in details this post ? 

https://community.st.com/t5/stm32-mpus-products-and-hardware/change-default-tf-a-and-u-boot-serial-linux-console/m-p/195027/highlight/true#M5675

 

Regards.

 

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
DMårtAuthor
Lead
January 29, 2026

Hi @PatrickF 

I have look at the details of this post.

The ETZPC is only available for MP1.

Do you think op-tee is blocking TF-A? Like something is blocking USART6.

It seems that a lot of people on this forum having issues with USART6 when I reading the threads.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
DMårtAuthor
Lead
January 29, 2026

I found an weird bug. I cannot change this value. Even if it's wrong.

DMrt_0-1769706690488.png

 

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
Kevin HUBER
ST Employee
January 29, 2026

Hello @DMårt 

 

To fix the wrong memclk value in your DDR configuration, you have to go in "Clock Configuration" tab and update the clock divider going "To DDR", around PLL2 clock mux.

 

Hope it helps,

BR,

Kevin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
DMårtAuthor
Lead
January 29, 2026

Hi @Kevin HUBER 

I have set my DDR to 600 MHz in the clock configuration tab so the memclk becomes 1200 MHz.

I will now see if USART6 is working as early boot debug. Perhaps not...

Edit:

It did not work.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
DMårtAuthor
Lead
February 7, 2026

@PatrickF @Kevin HUBER 

Here is the correct settings for USART6 for early console. I was misstaken for DEBUG_UART_TX_GPIO_ALTERNATE should have the number 8, i.e AF8, but according to the datasheet, it must have number 3, i.e AF3.

/* USART6 on HSI@64MHz, TX on PF13 Alternate 3 */
#define STM32MP_DEBUG_USART_BASE USART6_BASE
#define DEBUG_UART_TX_GPIO_BANK_ADDRESS GPIOF_BASE
#define DEBUG_UART_TX_GPIO_BANK_CLK_REG RCC_GPIOFCFGR
#define DEBUG_UART_TX_GPIO_BANK_CLK_EN RCC_GPIOxCFGR_GPIOxEN
#define DEBUG_UART_TX_GPIO_PORT 13
#define DEBUG_UART_TX_GPIO_ALTERNATE 3
#define DEBUG_UART_TX_CLKSRC_REG RCC_XBAR8CFGR
#define DEBUG_UART_TX_CLKSRC XBAR_SRC_HSI
#define DEBUG_UART_TX_EN_REG RCC_USART6CFGR
#define DEBUG_UART_TX_EN RCC_UARTxCFGR_UARTxEN
#define DEBUG_UART_RST_REG RCC_USART6CFGR
#define DEBUG_UART_RST_BIT RCC_UARTxCFGR_UARTxRST
#define DEBUG_UART_PREDIV_CFGR RCC_PREDIV8CFGR
#define DEBUG_UART_FINDIV_CFGR RCC_FINDIV8CFGR

. Here is the output result:

NOTICE: Early console setup
ERROR: failed to enable clock id: 5
BACKTRACE: START: clk_stm32_enable_call_ops
0: EL3: 0xe017bac
1: EL3: 0xe01be2c
2: EL3: 0xe01beb0
3: EL3: 0xe01bf54
4: EL3: 0xe01c240
5: EL3: 0xe01db28
6: EL3: 0xe029a2c
7: EL3: 0xe0170dc
BACKTRACE: END: clk_stm32_enable_call_ops
PANIC at PC : 0x000000000e01be34

 

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer