cancel
Showing results for 
Search instead for 
Did you mean: 

GaN based half bridge board with gate driver

jrf_abhishek
Associate

Hello,
I am looking for GaN based half bridges or full bridges evaluation board with gate driver for 250-400V and 3.3kW power rating for Dual active bridge DC-DC converter.
Kindly suggest evaluation/ development board for the same

Thanks & Regards
Abhishek

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @jrf_abhishek, to the community!

I have just come across your older question: if it is still relevant, currently there is no GaN based solution for it from STMicroelectronics.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.