2020-06-01 9:01 AM
I need my 0.9 degree stepper motor to hit 3000 rpm, is this possible with the POWERSTEP01?
2020-07-22 3:11 AM
The value of 15610 step/s is the maximum speed allowed by the integrated motion engine (for example when the logic processing the SPI commands).
Using the Step-Clock mode (refer to stepclock command in the powerSTEP01 datasheet at page 76) you can overcome this limit.
In Step-clock mode the motor motion is defined by the step-clock signal applied to the STCK pin. At each step-clock rising edge, the motor is moved one microstep in the programmed direction and absolute position is consequently updated
Maximum step-clock frequency is about 1.5 MHz.