cancel
Showing results for 
Search instead for 
Did you mean: 

FOD on STWBC-MC

SvenRaecker
Associate

 

Hello STM community.

We developed a wireless charger based on the STWBC-MC chip.

Our design follows exactly the ST Eval-Kit STEVAL-ISB047V1.

No we are facing a problem with a customer, that the Foreign Object Detection (FOD) does not work stable. In some cases the charger does not detect foreign objects and still transfers power, wich resulted in one case to an overheating of the charging surface (deformation, melting marks and smell).

 

Is there a chance to improve the FOD by tuning the parameters (see picture below)? The description of the parameters is unclear for us and does not help. How can we evaluate proper parameters?

 

Thanks in advance,

Sven.

SvenRaecker_1-1710136601114.png

 

 

 

3 REPLIES 3
willzhou
ST Employee

Hi

please check this document to change fod setting.

BTW our wireless charge product have updated.

https://www.st.com/content/ccc/resource/technical/document/user_manual/group1/a2/fc/ce/c3/9f/e4/40/8a/DM00550209/files/DM00550209.pdf/jcr:content/translations/en.DM00550209.pdf

 

https://www.st.com/en/power-management/stwbc2-hp.html

 

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SvenRaecker
Associate

Thanks for you answer.

I know this document. Section 5.2.2 describes the QFOD calibration procedure (Test 2").

But additionally I'd like to understand, what the parameters in the registry settings are used for. Is there a chance to adjust the FOD performance/sensitivity? The registry description does not help to understand it.

In the "Test" menu, there is also a "FOD metrics" function. 

I understand that, if the FOD margin goes under 0, the FOD is active and turns of charging. But what are the other parameters? Can I use that to evaluate a proper FOD sensitivity.

Our application uses different coversheets between the charging surface and the smartphone. I understand that this requires a tuning to adjust the FOD.

SvenRaecker_0-1710420277578.png

 

Thanks and best regards, Sven.

willzhou
ST Employee

Hi

If your application uses different coversheets, please use the worse coversheets, for example maximum thickness coversheets, use GUI and Section 5.2.2 to do QFOD calibration.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.