cancel
Showing results for 
Search instead for 
Did you mean: 

eval-L6470 firmware

jimmjimmshen
Associate III
Posted on November 12, 2015 at 10:50

hi, i want to know where can i get the source code for eval-L6470 board default firmware? i got fwpspin_discoveryboard_v205.hex file, it work but shows error light i want to trace the error so i need the source code. i only find firmware with library project but i looks little different with fwspin one

3 REPLIES 3
dlindstrom13
Associate
Posted on November 12, 2015 at 21:18

what error light are you talking about?

jimmjimmshen
Associate III
Posted on November 13, 2015 at 01:40

In the case the ready led and error led switch on and not blinking. i read the user manual it shows:

– either the board ID is not recognized by the FW (bad FW versions used)

– or there is a problem with the SPI (no connection between the MCU and the L6470

via the SPI)

– or there is no 5 V - 45 V DC power supply.

i'm sure the power supply is fine then i replace the L6470 chip problem still there.

Gigi
ST Employee
Posted on January 07, 2016 at 18:23

Ciao

For question regarding stepper motor control I suggest to try this forum

https://my.st.com/public/STe2ecommunities/motordriver_ics/Lists/Motor%20Driver%20ICs%20and%20Boards

Ciao

Gigi