2024-11-27 06:43 AM
I just bought 10 pcs of LDL1117S33R which i plan to use them to power 3.3V modules form a 4V regulated source.
According to the data sheet the typical dropout is 350mV and max is 600mV @1.2A. My module consumes less than 500mA, so i expect to have enough margin with a Vin of 4V to get 3.3V at the ouput. But the module doesnt boot at 4V input.
When measured the dropuout is 1V - 1.1V. Did anybody face this problem?
The chips are labeled LL33 F329 with ST logo
Solved! Go to Solution.
2024-11-27 07:28 AM
@ves011 The max 600mV for the LDL1117 is specified for an input voltage that is at least 1V above the output voltage. With your small voltage difference, I would recommend switching to an ultra-low dropout LDO, e.g. the LD39100PU33R.
Regards
/Peter
2024-11-27 06:52 AM
2024-11-27 07:00 AM
@Andrew Neil wrote:
Often the current required to boot is more - sometimes much more - than the operating current ...
Called "inrush current" :
https://www.matsusada.com/support/terms/ps/rush-current.html
2024-11-27 07:08 AM
Here is the boot current captured with power monitor
its 60mA. Later on when WiFi is enabled and communication starts it has spikes of ~500mA
2024-11-27 07:19 AM
To make it more clear, with 4V input the output is 2.94V which is more than 100mV below the rated output.
2024-11-27 07:22 AM
What is the voltage output with no load?
2024-11-27 07:26 AM
Show your schematic
2024-11-27 07:28 AM
@ves011 The max 600mV for the LDL1117 is specified for an input voltage that is at least 1V above the output voltage. With your small voltage difference, I would recommend switching to an ultra-low dropout LDO, e.g. the LD39100PU33R.
Regards
/Peter
2024-11-27 07:31 AM
when Vin > 4.4V, Vout is steady 3.369V. I tested it up to 6V
Vin Vout
4.3 - 3.236
4.2 - 3.138
4.1 - 3.040
4.0 - 2.942
all these on a constant load of ~20mA
2024-11-27 07:38 AM - edited 2024-11-27 07:40 AM
What @Peter BENSCH said confirmed your findings.
4.3 - 3.236 = 1,064V
4.3 - 3.236 = 1,062V
4.1 - 3.040 = 1,06V
4.0 - 2.942 = 1,058V
.
.