cancel
Showing results for 
Search instead for 
Did you mean: 

droput voltage for LDL1117

ves011
Associate

I just bought 10 pcs of LDL1117S33R which i plan to use them to power 3.3V modules form a 4V regulated source.

According to the data sheet the typical dropout is 350mV and max is 600mV @1.2A. My module consumes less than 500mA, so i expect to have enough margin with a Vin of 4V to get 3.3V at the ouput. But the module doesnt boot at 4V input.

When measured the dropuout is 1V -  1.1V. Did anybody face this problem?

The chips are labeled LL33 F329 with ST logo

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

@ves011 The max 600mV for the LDL1117 is specified for an input voltage that is at least 1V above the output voltage. With your small voltage difference, I would recommend switching to an ultra-low dropout LDO, e.g. the LD39100PU33R.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

11 REPLIES 11

@ves011 wrote:

My module consumes less than 500mA


How is that determined? Is that the average operating current?

 


@ves011 wrote:

But the module doesn't boot at 4V input.


Often the current required to boot is more - sometimes much more - than the operating current ...


@Andrew Neil wrote:


Often the current required to boot is more - sometimes much more - than the operating current ...


Called "inrush current" : 

https://www.matsusada.com/support/terms/ps/rush-current.html

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Here is the boot current captured with power monitorScreenshot 2024-11-27 170250.png

its 60mA. Later on when WiFi is enabled and communication starts it has spikes of ~500mA

To make it more clear, with 4V input the output is 2.94V which is more than 100mV below the rated output.

What is the voltage output with no load?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Show your schematic

Peter BENSCH
ST Employee

@ves011 The max 600mV for the LDL1117 is specified for an input voltage that is at least 1V above the output voltage. With your small voltage difference, I would recommend switching to an ultra-low dropout LDO, e.g. the LD39100PU33R.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

when Vin > 4.4V,  Vout is steady 3.369V. I tested it up to 6V

Vin   Vout

4.3 - 3.236

4.2 - 3.138

4.1 - 3.040

4.0 - 2.942

all these on a constant load of ~20mA

 

 

What @Peter BENSCH said confirmed your findings.

SofLit_1-1732722026157.png

4.3 - 3.236 = 1,064V

4.3 - 3.236 = 1,062V

4.1 - 3.040 = 1,06V

4.0 - 2.942 = 1,058V

.

.

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.