2017-02-13 11:46 AM
I want to use the STM6600 controller to manage the power ON/OFF of my microcontroller system. In the specific I want:
- Turn ON the system simply pushing a button.
- Turn OFF the system simply pushing the same button.
- Force the power OFF pushing and holding the same button.
I read at pg. 5 on the STM6600
that'By a long push of one button (#PB) or two buttons (#PB and #SR) either a reset is asserted or power for the application is disabled depending on the option used.'
It says that pushing one button (#PB) OR two button
(#PB and #SR) I can disable the main power
Then at pg. 10 it says
'A short push of the push-button during normal operation can initiate an interrupt through
debounced #INT output (see Figure 14) and a long push of #PB and #SR simultaneously caneither assert reset output #RST (see Figure 18) or deassert the EN or #EN output (seeFigure 19) based on the option used.'In this case it says that, to disable the EN signal, I have NECESSARILY to push two button: the #PB and the #SR simultaneously.
Now I'm a bit confused. If I want use only one push button to have the behaviour described above, I have to connect to ground permanently the #SR input of the STM6600 controller?2017-02-16 2:50 PM
Can anyone help me?