cancel
Showing results for 
Search instead for 
Did you mean: 

L6472, problem with absolute position register

Jacob Heder
Associate
Posted on February 10, 2017 at 15:10

Hi

I'm using the L6472 Eval board, revision 1.1.

We got two 

L6472 Eval board connected to our main stm32f2 board. Both drivers are 

running smoothly and everything is working, but reading the absolute position register makes no sense.  The absolute register seems to have some faulty bits, which is hardwired to 0.  I'm using the c driver which weremade by ST. (dspin.c)

When reading the absolute position register (called ABS_POS in the datasheet) is in 2's complement format and it ranges from -2^21 to +2^21-1.  I'm using the 

dspin.c driver to read this value (see below) but I do not get the correct value.  

I'v also got the new L6472 DISC eval board and tryed it via windows and here the ABS_POS seems to work.

I'm currently moving the motor without checking if my position is correct. However due to safety reason I need to

known the absolute positon.

Is this an chip issue on some older chips ? ..  Any workarounds ?

Regards Jacob.

--- 

/* Issues dSPIN Get Param command. */

uint32_t dSPIN_Get_Param(dSPIN_Registers_TypeDef param)

{

int32_t temp = 0;

int32_t rx = 0;

/* Send GetParam operation code to dSPIN */

temp = dSPIN_Write_Byte((uint8_t)dSPIN_GET_PARAM | (uint8_t)param);

/* MSB which should be 0 */

temp = temp << 24;

rx |= temp;

switch (param)

{

case dSPIN_ABS_POS: ;

case dSPIN_MARK: ;

case dSPIN_SPEED:

temp = dSPIN_Write_Byte(device,(uint8_t)(0x00));

temp = temp << 16;

rx |= temp;

case dSPIN_EL_POS: ;

case dSPIN_ACC: ;

case dSPIN_DEC: ;

case dSPIN_MAX_SPEED: ;

case dSPIN_MIN_SPEED: ;

case dSPIN_FS_SPD: ;

case dSPIN_CONFIG: ;

case dSPIN_STATUS:

temp = dSPIN_Write_Byte(device,(uint8_t)(0x00));

temp = temp << 8;

rx |= temp;

default:

temp = dSPIN_Write_Byte(device,(uint8_t)(0x00));

rx |= temp;

}

return rx;

}

#absolute-position #l6472
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Enrico Poli
ST Employee
Posted on February 16, 2017 at 12:27

Hi,

the ABS_POS register is basically a 22 bit counter.

When you read it through the SPI 3 bytes are returned (24 bits), so the two MSbits are always low.