2024-10-10 01:11 AM
Hello,
I have a question regarding the L9800 product (LS driver). The value of the CFG_2.FR_ADJ bit in "Table 12. Coefficient overview" differs from the value of the CFG_2.FR_ADJ bit in "Table 18. Register addressing space" in the datasheet. Could you please clarify which value is correct?
* Table 12. Coefficient overview
* Table 18. Register addressing space
Thank you.
2024-10-18 03:57 AM
Hello,
you are right, there is a mismatch between table 12 and table 18. The right values are the ones inside the table 12.
Our team will change the datasheet information included in the table 18.
thanks
Giulia