Hello, you are right, there is a mismatch between table 12 and table 18. The right values are the ones inside the table 12.Our team will change the datasheet information included in the table 18.thanksGiulia
Hello,The gate current is internally limited to value reported in table 15 that can be considered as peak value, so also applying 0Ohm resistor to gate there is no risk to damage the device.In fact, with configuration GCC[1:0] = [1, 1], [1, 0], [0, 1...
Hello Yang,i will suggest you to see the paragraph 2.5 of the Application note AN5311 that you can download from the st.com page related to L9945.It's possible to choose different dead time values for both H-bridges independently to prevent cross-con...