2012-02-03 6:20 AM
I have STEVAL-ISF002V1 digital PFC board and STM3210E-EVAL. Can i directly drive PFC board without modifications on the two board?
2012-05-16 2:18 AM
Hello,
you can read UM0877, section 7.3 about jumper settings for the two boards. For digital PFC and motor control (single/dual), stay tuned because it's coming soon a new integrated ST evalboard with PFC (discrete), IPM for motor(s), STM32 and a PFC software library plug-in for STM32 PMSM SKD v3 Best regards, Dino2013-07-08 10:50 AM
This thread is quite old. Any news/progress on this topic (digital PFC + STM32 PMSM SKD v3)? Is any source code available?
2013-07-09 6:26 AM
Hello,
the evaluation board mentioned in this thread it is this:http://www.st.com/web/catalog/tools/FM116/SC1077/PF253934?s_searchtype=partnumber
The firmware is in qualification. Ciao Gigi