cancel
Showing results for 
Search instead for 
Did you mean: 

Digital PFC with STM3210E-EVAL

ahmetnas
Associate
Posted on February 03, 2012 at 15:20

I have STEVAL-ISF002V1 digital PFC board and STM3210E-EVAL. Can i directly drive PFC board without modifications on the two board?

3 REPLIES 3
Dino COSTANZO
Associate II
Posted on May 16, 2012 at 11:18

Hello,

you can read UM0877, section 7.3 about jumper settings for the two boards.

For digital PFC and motor control (single/dual), stay tuned because it's coming soon a new integrated ST evalboard with PFC (discrete), IPM for motor(s), STM32 and a PFC software library plug-in for STM32 PMSM SKD v3

Best regards,

Dino

tomtom9197
Associate II
Posted on July 08, 2013 at 19:50

This thread is quite old. Any news/progress on this topic (digital PFC + STM32 PMSM SKD v3)? Is any source code available?

Gigi
ST Employee
Posted on July 09, 2013 at 15:26

Hello,

the evaluation board mentioned in this thread it is this:

http://www.st.com/web/catalog/tools/FM116/SC1077/PF253934?s_searchtype=partnumber

The firmware is in qualification.

Ciao

Gigi